6/25/2014 11:58 AM | |
Posts: 2 Rating: (0) |
Dear Support team, SiPass ACC5102 Technical Manual states that RS485 bus connected on ACC5102 controler shall be connected to +5 V wheras POWER is already provided from the ACC5102 LNF interface... Can you explain why we need 5 V? Where can I get the source of 5 V on the ACC5102 ? See page 17 of Technical Manual attached. Many thanks Regards
AttachmentSiemens_AC5102_technical manual.pdf (741 Downloads) |
6/26/2014 12:52 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
closed cause question posted twice. The second thread with the subjectSiPass ACC5102 - Connection with RS485 busis published within the conference Desigo™ Building Automation System. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on