6/23/2014 5:25 PM | |
Posts: 2348 Rating:
|
If you are looking function, that sums some working hours try searching "totalizer" here on forum and use standard library (File-Open-Library-...) |
6/23/2014 9:26 PM | |
Posts: 5225 Rating:
|
Hi. Sorry for the late reply. I am a bit surprized that an expert did not come forward with an answer that pushes you in the right direction. My contribution to this thread was to help things along.. getting the conversation started for the experts to swoop in with an answer. It has been a while for me using Step7 V5.x and S7-300 / 400 system. What you need I have had the need to use. However.. please find attached a printout which I think might help. It comes form the help inside TIA, but it should still apply. I think when you use this time delay interrupt, you will not need to add time. -- that is unless I have misunderstood the final goal. I ask you to have a look at the PDF and follow up on the relevant literature ("System Manual") for your CPU. Please get back to this foru with your thoughts and hopefully there will be someone her with a helpful answer. Good luck. w AttachmentTime delay interrupt OB.pdf (91 Downloads) |
6/25/2014 11:18 AM | |
Joined: 11/3/2013 Last visit: 12/14/2021 Posts: 18 Rating:
|
Hi there are no totalizer to add following format DATe_TIME & Hours regards Sajit |
7/3/2014 11:09 PM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating:
|
|
Follow us on