7/14/2014 11:12 PM | |
Posts: 5225 Rating:
|
touché! [smile] It is difficult to have this conversation.. it is a bit of a guessing game to know what your background is. You will have to develop the background coding yourself. You could however try something from OSCAT [LINK] and convert it to SCL. Process control is not my field of practice for a long time. I do however remember that flow through a valve is not always linear in relation to how big the valve is open and that pressure in the system play a big role. Measuring flow of water is easy in comparison to measuring the flow of acid. -- I can not help but being concerned about these factors. There is also the case of how the system reacts on a power outage / PLC failure / PLC error and such things. In my book the writing of code is easy when compared to engineering the process well. If I may leave the engineering in your hands.. my opinion for the PLC side is that the S7-1200 will be able to handle the process control, but you will have to much of the coding to do yourself (excluding the PID loop(s) ). The S7-1200 is capable of handling the maths and the analogs. I recommend you to refrase this question and ask the forum's opinion which PLC is best suited for the job you have in mind. The "SIMATIC S7 general" would be the best place for this question. If you could state what sensors and actuators you plan to use and signal type (analog/communications), this will be most helpful. Good luck w |
7/24/2014 1:07 AM | |
Posts: 3 Rating:
|
Thanks Williams. |
7/25/2014 7:00 PM | |
Posts: 3 Rating:
|
Hi Mark, That's really helpful. Thanks for the explanation. I am trying to make it work in this direction. |
This contribution was helpful to
1 thankful Users |
Follow us on