8/22/2014 8:41 AM | |
Posts: 2 Rating: (0) |
Dear Experts, In one project I want to communicate 3X S7-412-5H PLC system with 3X standalone Wincc stations. Please see attachment for automation configuration. System details are as follows- 1. I want to use PN port of H CPU for communication with Wincc 2. I want communicate all 3 H CPU systems with each stand alone Wincc HMI station (data of all 3 H system should display on each hmi station). 3. I have consider 1X CP1623 and 1X S7 REDCONNECT software for each HMI station PC. 4. I don’t want redundancy at HMI station/ CP1623 Or network. So my queries are as follows- 1. This configuration will work or not? 2. How Wincc will come to know from which CPU (H1 or H2) in each s7-400H system it should get data? (Means if 1st CPU (H1) of H system fails 2nd CPU (H2) will take control of IOs but how wincc will also start taking data from H1) AttachmentC:\Users\in213696\Desktop\H-PLC_AUTOMATION_CONFIGURATION_Rev00.pdf (137 Downloads) |
Follow us on