10/15/2007 11:15 AM | |
Posts: 5822 Rating: (411)
|
Dear phneutre, well, if you have a CP 342-5 DA02 this can be done. Older CP's do not support active S7 Communication. Best regards J_Bell |
10/15/2007 11:30 AM | |
Posts: 5 Rating: (0) |
Yes the two CP 342-5 are DA02. |
10/15/2007 12:34 PM | |
Posts: 5 Rating: (0) |
The way to proceed is it the same as an example CP343-1
|
10/18/2007 10:50 AM | |
Posts: 5 Rating: (0) |
Ok thank you |
Follow us on