8/26/2014 11:50 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, If there is not a CP 5622 in the hardware catalog of your STEP 7 version , you can select a CP 5621 or CP 5611 for configuration. If you have Step 7 SP3 you can download a HSP here; STEP 7 V5.x Hardware Support Packages (HSPs - as at 08/2014) for installing hardware updates in the Hardware Configuration Regards, Marcjan |
Last edited by: Marcjan at: 8/26/2014 11:55 AMProblem solved? |
|
8/26/2014 12:32 PM | |
Posts: 102 Rating: (2) |
Thank you so much for such a quick response ! Appreciated! |
This contribution was helpful to1 thankful Users |
Follow us on