9/3/2014 1:06 PM | |
Posts: 1058 Rating: (93) |
Maybe this link will help you: Dispay local date and time in WinCC Professional V11 RT I guess the clock function could be useful to your application too. regards |
9/3/2014 1:15 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2146) |
Hello zga, in the FAQ 7802886 kann you find a C-script for reading the Systemtime of a PC. http://support.automation.siemens.com/WW/view/de/7802886 |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
9/3/2014 3:37 PM | |
Joined: 4/19/2011 Last visit: 2/12/2024 Posts: 37 Rating: (3) |
Thanks for the reply. Is it possible to write same code in VBS. |
9/4/2014 8:07 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2146) |
Hello zga, you can use VBS in a similar way too. in the FAQ59558655 part 3you can find a description. http://support.automation.siemens.com/WW/view/en/59558655 Or the Now function |
PS: If this post did really help you, you may use the Rate-button |
|
9/4/2014 3:16 PM | |
Joined: 4/19/2011 Last visit: 2/12/2024 Posts: 37 Rating: (3) |
Hellobg2492, How to get the Minute in VBS to compare it with "00".
|
Follow us on