(0)| 9/19/2014 1:45 PM | |
|
Posts: 1 Rating:
|
Hi, can SITRANS FUE950 provide mass(flow, volume) values in addtion/exchange to volumetric(flow, volume) values ? Thanks |
| 9/19/2014 3:24 PM | |
|
Joined: 12/11/2012 Last visit: 1/16/2026 Posts: 35 Rating:
|
No, this is not possible. |
| 9/19/2014 6:39 PM | |
|
Joined: 3/28/2010 Last visit: 1/21/2026 Posts: 1210 Rating:
|
I don't see where the FUE950 gives a mass flow reading. I only see volumetric flow readings. I skimmed the manual and the flow rates are listed in examples as m3/hr, which is volumetric. The catalog sheet here, http://w3app.siemens.com/mcms/infocenter/dokumentencenter/sc/pi/InfocenterLanguagePacks/Catalog%20sheet%20SITRANS%20FUE950/sitransf_fusfue950_fi01en.pdf says, Units: MWh, GJ, Gcal, MBtu, m3, gal, m3/h, GPM, °C, °F and kW; all decimal points are statically (the unit "gal" is shown with factor x 100). "The main menu loop no. 1 with the current data, e.g. for energy, volume, flow rate and temperature, is preprogrammed as default setting." Values stored • Energy • Volume • Tariff counter 1 • Tariff counter 2 • Pulse counter 1 • Pulse counter 2 • Date The manual (May 2014) says, "In the normal operation menu loop, the display will show accumulated energy and volume as well as the actual flow and temperature values." Where's the mass units? |
Follow us on