9/11/2012 10:26 AM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Greeting, First Issue: I have connected 8 Modbus devices with WinCC flexible i have creat 5 tags for each device total number of tags for 8 devices on 1 screen is 40 when i start runtime the some tags value is converting in ###### but when i shift 20 tags from this screen to another screen the problem is solve what will be reason see attached result of both screen..?? I am using CPU type Premium, Micro. Second Issue: Could you explain how can i create 72 modicon modbus TCP/IP connection in wincc flexible..??? Because when i creat 9th connection Software giving a message "Maximum Number of Connection for the Interface Exceeded"..???? Thanks. Regards. AttachmentDesktop.zip (60 Downloads) |
Last edited by: Sarfraz Bhatti at: 9/11/2012 12:09 PMMS |
|
9/11/2012 12:55 PM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello, Are you using a Panel? What are the update cycles of the tags? Best regards, Wizard |
9/11/2012 1:31 PM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Greeting, I am using Runtime on local PC and update cyle is 5 Sec. Thanks. Regards |
MS |
|
9/14/2012 8:09 AM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Greeting, yes, i have delete temporary files but problem is still ..?? Thanks, Regarded |
MS |
|
9/14/2012 9:34 AM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Yes result is better when i use 20 sec cycle time. |
MS |
|
9/14/2012 11:24 AM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating: (11) |
Greeting Please see attached how can i use in group and sequentially..??? Thanks, |
MS |
|
9/24/2014 3:04 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published byBAYRAK Ayseis split to a separate thread with the subjectmodbus problem about 72 connection. Best regards Min_Moderator |
Follow us on