9/28/2014 5:13 PM | |
Joined: 9/27/2006 Last visit: 9/26/2024 Posts: 12283 Rating: (2685) |
Hello K.C. First thing, for any WinCC project, you need a Configuration/Runtime package in order to create your project: an RCxxxx license (where xxxx represents the number of tags you want to control). For example: WINCC SYSTEMSOFTWARE V7.2, RC 65536 (65536 POWER TAGS), RUNTIME & CONFIGURATION -SW FLOATING LICENSE, SW AND LICENSE KEY Then you can install the project on Server licenses, one license per server (you must purchase 2): WINCC/SERVER V7.2, OPTION FOR SIMATIC WINCC V7.2, RUNTIME SOFTWARE, SINGLE LICENSE If you want redundant servers, each server must have a redundancy license; the WinCCredundancy option contains 2 licenses. WINCC/REDUNDANCY V7.2, OPTION FOR SIMATIC WINCC V7.2, RUNTIME SOFTWARE, SINGLE LIC. F. 2 INSTALLATIONS Clients can be setup with the smallest of runtimetag licenses, no matter what number of tags has been used in the project: a RT128 license; you need one per WinCC client station: WINCC SYSTEMSOFTWARE V7.2, RT 128 (128 POWER TAGS), RUNTIME-SW, SINGLE LICENSE, SW AND LICENSE KEY One place you can find product descriptions and part numbers isin the Siemens Industry Mall (Electronic Catalog), from which the attached screenshot is taken: https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/10013016?tree=CatalogTree Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
9/30/2014 8:52 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
Follow up question published by K C Dasis split to a separate thread with the subject Informations about WinCC. Best regards Min_Moderator |
Last edited by: Min_Moderator at: 9/30/2014 9:01 AM |
|
Follow us on