10/14/2014 1:12 PM | |
Joined: 5/12/2006 Last visit: 10/14/2024 Posts: 22411 Rating: (3017)
|
Hi, it is much better if you read the relevant documentation! SIMOTION have no control word or status word! SIMOTION is a PLC with program logic for Motion Control Applications. For the coupling aof a S7 with a SIMOTION you should refer this document. Regards Christoph |
10/14/2014 11:34 PM | |
Posts: 7 Rating: (0) |
Thank you for the good help |
10/23/2014 7:19 AM | |
Posts: 153 Rating: (8) |
I did this before setting SIMOTION as an I-Device and using SFC14 and 15 in the S7. It works fine. See this example. Attachment38494882_Application_Example_RT_I-Device_V1_3_en.pdf (314 Downloads) |
Last edited by: Min_Moderator at: 10/23/2014 2:02 PMMove link to attachment |
|
Follow us on