10/30/2007 9:36 AM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12408 Rating:
|
Hello sreeram; To communicate to a PG with SI 2 interface, you will need a "PG Submodule" (part no. 6ES5 752-0AA53) and a 6ES5743-2xxx0 cable (with TTY converter, as you pointed out). These are not listed on Siemn's A&D Mall anymore, but you can find them, used or repaired, from special dealers. Google led me here: http://www.classicautomation.com/catalog/productdetail.aspx?partnum=6ES5752-0AA53 Hope this helps, Daniel Chartier |
11/1/2007 10:35 AM | |
Posts: 3 Rating:
|
Hello Sreeram, If u r in india, the TTY converters are available at Renu Electronics,PUNE or Fox Controls, Nashik. Regards, |
11/1/2007 7:31 PM | |
Posts: 5822 Rating:
|
Hello, there are some TTY interfaces, active or passive, available on the Internet. Also units with USB interface... just take a look. Best regards J_Bell |
11/2/2007 2:10 PM | |
Posts: 53 Rating:
|
Dear Buddies, Thanks a lot for your support. Will get back to you shortly after checking it up with the sources. Regards Sree |
Follow us on