11/12/2014 8:57 AM | |
Joined: 6/26/2013 Last visit: 4/23/2024 Posts: 143 Rating: (5) |
Hello Please find attached parameter list. P373=0 Regards AttachmentF:\MASTERDRIVES VC(CUVC)_tm.zip (196 Downloads) |
meeda_ |
|
11/12/2014 10:26 AM | |
Joined: 10/11/2006 Last visit: 9/9/2024 Posts: 5902 Rating: (803)
|
Hello meeda, reset is connected to the communication and to DI1 in Dataset 2 (active if DI2 is set). We found also, that there were many DC link undervoltage faults stored. You should make a trace with fault active as trigger and trigger on the control word and communication to find out, where the reset comes from. It could be helpful to contact the customer support. |
With best regards, |
|
Follow us on