11/28/2014 2:58 AM | |
Posts: 17 Rating: (0) |
hello bg2492, this is what i am referring to.. i wanted to display the runtime data in the table window..
|
11/28/2014 2:58 AM | |
Posts: 17 Rating: (0) |
hello bg2492, this is what i am referring to.. i wanted to display the runtime data in the table window..
|
11/28/2014 6:18 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2146)
|
Hello KSooH, your screenshot show a correct working project. The button with the "grid" is set, and the data are displayed. I know only a situation, when the Userarchiv-Editor was not correctly closed before, the file "UAEditor.loc" in the WinCC-projectfolder was not deleted, an the Editor is writeprotected, if you open it again. see: http://support.automation.siemens.com/WW/view/en/492977 If this is not your situation too, I guess the project is inconsistent. You should create a Support Request, and send the project to the Technical Support for investigation. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
Follow us on