(2)| 12/15/2014 1:27 AM | |
|
Posts: 510 Rating:
|
If you are using Portal V13, there is a new feature called the "Proxy PLC". This lets you configure a PLC in V13, update the tags from Step 7 V5.5 and connect with the HMI. I developed a class earlier this year on the new features of V13 and the panels, Basic Panels 2nd Generation and Comfort panels. I have attached the portion of the slides that dealt with the "Proxy PLC" Unfortunately the demo kits for the class did not include an S7-300 so the screen captures are for TIA Portal (S7-1215) but the process is the same. I hope this will assist you in your efforts. Good luck, billwest AttachmentPLC for HMI.pdf (381 Downloads) |
Last edited by: Min_Moderator at: 12/15/2014 11:15 AMChange name of attachment Last edited by: billwest at: 12/15/2014 1:32 AM |
|
| 12/15/2014 6:24 AM | |
|
Posts: 4620 Rating:
|
Hello krisbi, In addition to our friend billwest have a look: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x |
Last edited by: Ste39 at: 12/15/2014 6:25 AM |
|
Follow us on