6/12/2009 5:32 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
dear all Attachmentfiles.zip (532 Downloads) |
This contribution was helpful to3 thankful Users |
6/12/2009 7:36 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hi RAM81, Good job! Think this example will be helpful. Thank you for sharing your expirience with us. Best regards Hristo Mihalev |
6/15/2009 5:13 AM | |
Posts: 15 Rating: (0) |
Thanks for the experience sharing. |
6/15/2009 5:56 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi |
8/2/2009 9:43 PM | |
Posts: 54 Rating: (8) |
Hi Genesis,This is not “Easy Extend”. Easy Extend is used to describe start up procedures of additional machine equipment. The 802D sl provides that function to add user masks into the control. XML expressions will be used in both cases. It is released with the SP5 (see http://support.automation.siemens.com/WW/view/en/37341071). |
Follow us on