1/27/2015 1:47 PM | |
Posts: 1 Rating: (0) |
Hi, I have one dought. Maximum lenght profibus cable for speed 1.5Mb is 200m from Master-1(one end of the cable) to Slave-5 (another end of the cable), or fromMaster-1(one end of the cable)to Slave-1.(example on picture)
---------- New subject after splitting from Is OPC supported on 64-bit versions of Windows?. |
Last edited by: Min_Moderator at: 1/27/2015 4:09 PMSplitted |
|
1/27/2015 8:33 PM | |
Posts: 1058 Rating: (93) |
Hello utomation.siemens, I have seen exact same question and also answer to that question here: maximal cable lenght for MPI and PROFIBUS DP netwo maximum lenght of Profibus networksyou find here: Acceptable line length in PROFIBUS-DP networks regards |
Follow us on