(0)| 6/15/2010 7:27 AM | |
|
Joined: 3/21/2006 Last visit: 1/29/2026 Posts: 10248 Rating:
|
Hello, Take a look at SPPA-T3000 System Overview.It's not enough, but like presentation is good.Best regards, Hristo Mihalev |
| 6/15/2010 8:09 AM | |
|
Posts: 130 Rating:
|
Hi Umencho, Thanks for that information. Can you kindly guide me as to what are the major differences between SPPA T3000 and PCS7 ?? Regards, |
| 6/15/2011 4:28 AM | |
|
Posts: 1 Rating:
|
What type of facility you have? If gas turbines I might be able to help you. |
| 1/19/2013 9:30 AM | |
|
Posts: 30 Rating:
|
Dears, The difference between sppa t3000 and pcs7 is my question too. Any body could give me the answer? regards, |
| 1/19/2013 3:51 PM | |
|
Joined: 9/27/2006 Last visit: 1/30/2026 Posts: 12485 Rating:
|
Hello eemi; Both PCS 7 and SPPA-T3000 are DCS systems provided by Siemens, but offered by different divisions. Some of the hardware might be similar (Profibus-DP distributed I/Os for example) but the systems are incompatible. SPPA-Tx000 is part of the Energy division and it is oriented towards enegy generation (power plants) http://www.energy.siemens.com/hq/en/automation/power-generation/sppa-t3000.htm PCS 7 is a S7-400/WinCC based system developped for discrete and continuous process control, by the I&A division (Industry and Automation): |
| 3/8/2015 4:09 PM | |
|
Posts: 1 Rating:
|
Hi can anyone provide me complete PDF of SPPA T-3000 control system and oblige. rgds, |
Follow us on