(0)| 3/27/2015 7:51 AM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
It is not possible the whole address you mentioned in AR1 ( P#DB1.DBX46.0).This notation is similar to ANY pointer and requires 10 bytes of data or DB pointer.If you want to the task in iteration, use loops and if you need to work on 2 DBs , DB registers will help.To access an specific DB/DI use open command for each.I think check the sample codes in the following thread will help you.Try and update:
Copy bit from DBxxx to DByyy |
Follow us on