4/10/2015 12:02 PM | |
Joined: 4/12/2013 Last visit: 5/17/2024 Posts: 47 Rating:
|
Dear All, Our CNC Machine’s “Sinumerik 802C Baseline Controller” has failed. Detail: Manually all functions are working but Its screen is off because of CNC controller problem. On execution of user program, machine (was working ok previously but now) shows error but we cannot see error because of screen failure. Manually again, all functions are working. Remedy: So, we decided to replace “Sinumerik 802C Baseline Controller” with spare/new one. 1, We load backup program from machine vendor in “Programming tool PLC802C” and when press download to Controller then program is automatically compiled by “Programming tool PLC802C” but show error whose detail is attached in picture. No downloading starts. 2, We suspect that maybe backup program is corrupted. So, with some efforts we take backup from old CNC controller and try that program on new CNC controller. Although read program from old controller was successful but it show again same problem of compiling and no download to new controller is started. Please check and guide us.
Best Regards, jarrar AttachmentSinumerik 802C Baseline Controller Problem.zip (46 Downloads) |
Follow us on