4/16/2015 7:16 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating: (797)
|
Hello Comelec,
CUVC for RG3 has a special firmware for excitation systems, which is not compatible with the standard firmware for CUVC. You should contact the manufacturer of the RG3 system for a spare RG3 CUVC or to get the firmware files. If you have the firmware files for RG3 and standard CUVC (https://support.industry.siemens.com/cs/ww/en/view/24232156), you can use one CUVC as spare part, but need to load the correct firmware before use.
|
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on