5/5/2015 10:21 PM | |
Joined: 9/27/2006 Last visit: 8/8/2024 Posts: 12273 Rating: (2680) |
hello Proov; You have 2 questions, basically. 1. can the IM 361 hold communictaion processors so hey can conect to the CPU from a remote rack? Yes, it can; see this discussion:
TCP communication using CP343-1 on IM361 2. How to exchange data between the CP 341-3 and the integrated Profinet port of a S7-400 CPU.
Specially:
The communication connection for open communication via the integrated Industrial Ethernet interface of the CPU is established to block FB65 "T_CON". FB65 "T_CON" is called in the S7 program of the CPU. In this case, there is no need to configure a communication connection in NetPro. The communication connection can be cleared down specifically by calling the block FB66 "T_DISCON Hope this helps, Daniel Chartier |
Follow us on