5/9/2015 5:20 PM | |
Posts: 1 Rating: (0) |
Good afternoon, I want to write on internal memory of the LOGO! (Hardware type 0BA7.ES4) sending online command from PC using a standard TCP/IP socket connection. I want to change online the delay of Retentive On-Delay Block. This is possible? What port shoul I connect to? Thanks in advance, ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/11/2015 11:24:27 AMNew subject after splitting |
|
5/9/2015 5:40 PM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263) |
You can use additional software, such as those or this german side |
Follow us on