5/11/2015 12:13 PM | |
Joined: 11/9/2008 Last visit: 8/8/2024 Posts: 409 Rating: (6) |
Dear All, I want to know how repeater Works? I have attached pdf file for different condition please explain me. Step-1 Segment-1 will connect form CPU DP port to Repeater A1B1 switch position will be ON for segment-1 and Segment-2 is connected to ET-200M. Switch position is ON. Step-2 Segment-1 will connect form CPU DP port to Repeater A1B1 switch position will be ON for segment-1 and Segment-2 A2B2 is connected to ET-200M Module and A2'B2' is connected to another ET-200M .Switch position is OFF. Step-3 Segment-1 will connect form CPU DP port to Repeater A1B1. Segment-2 A1'B1' is connected toEt-200M. switch position will be OFF and Segment-3 A2B2 is connected to ET-200M Module and A2'B2' is connected to another Et-200M .Switch position is OFF. Please help me to understand how it will be work?? Regards, Yogendra G
AttachmentRepeater.pdf (134 Downloads) |
5/11/2015 12:46 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, what kind of repeater is this? Do you have an order No.? regards, |
FCK WAR! |
|
5/11/2015 2:23 PM | |
Joined: 10/21/2013 Last visit: 8/7/2024 Posts: 416 Rating: (28) |
Hi, pls find the manual chapter 5.4.. 1.if both terminating resistor is activated channel 2 and channel 4 are terminated since we dont have any connection in it. 2.if 2nd terminating resistor is off both channel 3 and channel 4 are in use. 3.if both terminating resistors are off all the channels are used. Attachmentrepeater.pdf (139 Downloads) |
Follow us on