1/3/2012 4:45 PM | |
Joined: 9/23/2005 Last visit: 9/11/2024 Posts: 4347 Rating: (1444)
|
Hi, here there is a sample programthat usesREAD_DBL. It copys the DB2 to DB3. The DB2 has a atribute "Only sotre in load memory" and could not be monitored online. To operate it, go to Watch_table_1: and set the "Start_to_read" variable. Expected efect: DB3 becomes values 111, 222, 333. AttachmentREAD_DBL.zip (1932 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to7 thankful Users |
9/13/2013 2:11 PM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating: (195) |
new question published by Pinosis split to a seperate thread with the subject Sample Program: READ_DBL need help. |
My Forum is the place to personalize your profile, |
|
5/11/2015 2:43 PM | |
Posts: 57 Rating: (8) |
Hi Pegaia. I made a program with READ_DBL and WRITE_DBL. But the write block compiles with error : "Network 1,The reference information is inconsistent. The block cannot be compiled." I described here the whole problem, with attached project. Do you have any S7-1200 write example? Thanks a lot. |
Follow us on