11/22/2011 2:26 PM | |
Joined: 11/3/2009 Last visit: 5/15/2024 Posts: 6 Rating: (0) |
Hello, I have problem with WinCC PDL Runtime crashing whit error "WinCC Graphics runtime has stopped working" In PDL log: // // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Full crash log see attached Project contains 2 redundant servers (Win Server 2008,WinCC V7.0 SP2)+ 3 clients (Win 7,WinCC V7.0 SP2) PDL Runtime crashing on clients and servers too (not at the same time). I think its project related problem, but cannot locate problem. Tried to check scripts, compile everything, convert pictures and other recomendations which have found on google but nothing helps. It crashing at random time, random action or even no action with mouse or keyboard taken. Some times runtime works few weeks without crash, sometimes crashing few times a day. Attachmentpdlrtseh.pdf (372 Downloads) |
9/16/2014 8:45 AM | |
Joined: 9/20/2011 Last visit: 8/23/2023 Posts: 45 Rating: (0) |
Halo, |
9/16/2014 9:40 AM | |
Posts: 8 Rating: (0) |
There was some unused objects (with action scripts) outside picture region. Eg picture size 800x120 but object located at x:1500 y:900 |
Follow us on