9/9/2014 3:20 PM | |
Posts: 94 Rating: (8) |
Dear Kaulquappe, Out of three PN ports of CPU I'm using one port for communication with PC (SCADA) can I use other port for Modbus TCP/IP communication.?? Regards, Arunraje |
Last edited by: Min_Moderator at: 9/9/2014 3:48 PMNew Subject after splitting from /tf/WW/en/Posts/107936#top |
|
9/9/2014 4:52 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Arunraje Yes, of course you can !! The IM 151-8 has three Physical RJ45 ports, however even if it had only one physical Ethernet port, still you can use multiple protocols on the same physical port. The twoprotocols that you want to use, utilise different logical ports and can be used simultaneously. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
9/9/2014 7:44 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
For Modbus TCP/IP protocol, of course you need a special license. Details are available in the link previously posted by Kaulquappe,
Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
6/27/2015 2:59 PM | |
Posts: 3093 Rating: (322)
|
yes, see also https://support.industry.siemens.com/cs/ww/en/view/103709414 |
This contribution was helpful to1 thankful Users |
Follow us on