8/3/2015 10:42 AM | |
Joined: 4/12/2013 Last visit: 8/22/2024 Posts: 47 Rating: (0) |
Dear All, I am using two MasterDrive MC with resolver feedback one for Conveyor as Master and other for Piston. Using F01 technology Conveyor drive run as control mode and Piston drive as Synchronous mode with CAM profile. In CAM profile upper limit is 985 LU and Lower limit is -2217 LU of piston according to the Conveyor position. When I run system at low speed piston works perfect as system speed increases upper and lower limit of piston reduce according to speed (i.e. 10% speed of Master piston limits 985 & -2217, 100% speed of Master Piston limits 580 & -1439) I attached parameter file of both drives. Main Conveyor (6ES7021-4EP50), 14.0 Amp, 5.5kW Piston A (6ES7023-8TP50), 37.5 Amp, 18.5kW
Regards,
Jarrar AttachmentPistonAok_020715.zip (193 Downloads) |
Follow us on