9/15/2010 3:50 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Hi what is the use of TH-IEA PRO and , is it integrated part of STEP7 or should be bought seperately? best regards |
9/15/2010 4:49 PM | |
Joined: 9/27/2006 Last visit: 5/27/2024 Posts: 12257 Rating: (2668) |
Hello hdhosseini; Start by looking at Umencho's answer on this thread: /tf/WW/en/Posts/39573 As you can see, the options TH (Technological Hierarchy) and IEA(import-export assistant)-PO (Process object) are part of PCS 7. Licenses are required to use their functionnalities. There is a version of IEA installed with WinCC, for import and export of texts, alarms... we used it in version 6.2, at least. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/6/2015 1:40 PM | |
Posts: 3 Rating: (3) |
And...: TH (and IEA-PO) can also be installed from Dvd Simatic Maintenance Station. |
This contribution was helpful to2 thankful Users |
Follow us on