8/17/2015 2:46 PM | |
Posts: 7 Rating: (1) |
Morning, I can't find the good way to read data inside a structure type of DB. It works nice with simple DB :
But it doesn't work with DB struct in attachment
Am I wrong with the notation ? Thanks AttachmentDB struct.txt (157 Downloads) |
Last edited by: Min_Moderator at: 8/17/2015 3:47:22 PMMove code to attachment |
|
8/20/2015 1:40 PM | |
Posts: 7 Rating: (1) |
Here is in attachement the right way to access the structure elements of the data block : More information : Page 406 : STEP 7 Basic V11.0 SP2 ; System Manual, 04/2012, Step 7 basic |
This contribution was helpful to2 thankful Users |
Follow us on