10/3/2015 12:48 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
In this simple sample, two trends are displayed on HMI start screen.
Note: Historical data retain values even after change screen / HMI Power off, but the Trend view object is not updated in real time (it is necessary to change the screen, for example, to show actualized values). For real time trends displays see “WinCC Basic V13 SP1 – Simple Sample: Real Time Trends” at https://support.industry.siemens.com/tf/br/en/posts/135197/)
Requirements: WinCC Basic V13 SP1.
Project with a minimum configuration (stop button, tags, etc. ).
Configuration main steps:
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
Application and tools Demo projects for HMI operator panels under WinCC V13 (TIA Portal) for Basic Panels (2nd generation) and Comfort Panels https://support.industry.siemens.com/cs/br/pt/view/96003274/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Images: Due a size/ format restrictions, the images are first compacted as images.zip and after that attached to a zip archive (data.zip).
Project: Due a size/ format restrictions, the project are first compacted as project.zip and after that attached to a zip archive (data.zip).
AttachmentData.zip (1371 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on