(0)| 10/16/2015 10:09 AM | |
|
Posts: 23 Rating:
|
Dear Sirs, For an urgent case, a STOCK 6RA8085-6DV62(V1.4) 600A drive was installed instead of a 280A 6RA8078-6DV62. After the orderd 280A 6RA8078-6DV62 (v1.4.1)being arrived, I exchange the drive and download the parametes which exported from 600A's, pick up the new order number as 6RA8078-6DV62..,modify P50076..etc. The strange thing is that the new unit seems still recognize itself as 6RA8085-6DV62. How come? Because of this, it leads to F60167(fan speed too low) and F60043(EMF for braking operation too high). It is still same eventhough I make a "Restore factory settings". Kindly give your opinions. Thank you! Jim Attachmentexchange of different 6RA80.pdf (498 Downloads) |
Follow us on