10/23/2015 1:59 PM | |
Posts: 5225 Rating: (1195) |
My findings are the same as yours. .. no such import is possible. Maybe it is possible for the hardware, The System Manual for the S7-1200 FW4.1 also makes no such mention. A few years back I was told that there was no plan to handle STL, With the restriction of use of S7-1200 vs S7-300 AND having SCL, A type of GRAPH (as in FESTO branded PLCs) is however a much different matter IMHO. w |
Last edited by: William_B at: 10/23/2015 2:17:13 PMadd link |
|
10/23/2015 4:38 PM | |
Posts: 8946 Rating: (999) |
Yes, that would also be helpful. |
Follow us on