(0)| 10/29/2015 8:35 AM | |
|
Posts: 1 Rating:
|
hi. i have a problem connecting SMC Linear Stepper (LEYG25MB-200-S1AP1) actuator with EM253. the problem is i use a cable that was provided with the motor driver(LECPAP1-LEYG25MB-200) to the plc. through their manual, the P0+ P0- and P1+ P1- are connect to the cable NP+ NP- and PP+ PP- respectively. when the program run, the subroutine POS_Run execute the program but no reaction to the stepper driver. can we get the wiring diagram between EM253 and LECPAP1-LEYG25MB-200. since i can't find them at EM253 position module manual wiring diagram (page 455-457) Thanks and regards Amerhaizat ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/29/2015 1:52:32 PMNew subject after splitting |
|
Follow us on