12/27/2015 11:00 AM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
Hi Amazingahmed You are right. As WinCC don´t have native Drivers for ABB, you must use OPC. I believe Kepware has drivers for ABB PLC´s So, you can Install Kepware/KepServer OPC Server in the same machine where is WinCC, to avoid DCOM. and then setup it. Regards JM |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on