2/17/2008 3:31 PM | |
Joined: 5/15/2006 Last visit: 3/6/2008 Posts: 7 Rating:
|
I configuredtwo S7300 Stationwith CP341. One I configured as Modbus Master and one as Modbus Slave. I interconnected both the CP341 (one master & other slave). I was able to successfully send data from Master to Slave using Modbus Function 16 (i.e. Preset Multiple Registers). But I am unable to receive the data from Slave using Function 04 (Read Input Register). Can someone please tell me what is that I am missing. I am attaching the archived Step7 project for both the station as refrence. AttachmentCp341_te.zip (696 Downloads) |
Follow us on