2/4/2008 10:48 AM | |||||||||||
Posts: 124 Rating:
|
Maybe the CPU S7-300is not the better choice. You could do what you want with a CPU S7-400, CP 443-5 and PDM - with these you could setparameters fromSimocodes and Micromasters (limitedscope) from a Central Engineering Station. See this:
But maybe you can use this yet:
But I suggest you to talk with the Hotline / Technicall Support to verify all conditions and restrictions of your project (CPU, number of nodes, what you have to parameterize, etc). Good Luck |
||||||||||
2/11/2008 9:52 AM | |
Posts: 739 Rating:
|
Dear Mario, it is possible to control the MM4 direct by using S7. The easiest way to do it is to use the tool DriveES.Please find some explanations at link: http://support.automation.siemens.com/WW/news/en/22078757 http://support.automation.siemens.com/WW/news/en/22318171 http://support.automation.siemens.com/WW/news/en/23322610 http://support.automation.siemens.com/WW/news/en/22794082 |
Last edited by: JensS at: 11.02.2008 09:55 |
|
Follow us on