1/21/2016 7:45 AM | |
Joined: 2/21/2014 Last visit: 8/13/2024 Posts: 652 Rating: (348)
|
Hi, I am not sure about other things but I find two problems in string manipulation: first thing: Gets() function ? I think you can remove it. second thing: strcpy (strTag1,"charMachine"); in this statement, "charMachine" is a TAG name. you need to get the TAG value using GetTag function. see below char strTag1[100], strTag2[100]; Note: please take care of the string lengths. it is safer to use strncpy, strncat function. and I will take strTag1 string bigger then the size of strTag1 and strTag2 combined. you may need to put proper checks for empty string if required. I hope this helps. Thanks, HarrY |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
1/21/2016 1:18 PM | |
Joined: 1/15/2016 Last visit: 9/11/2024 Posts: 178 Rating: (4) |
Thank you for your answers. |
Follow us on