5/11/2015 8:48 AM | |
Posts: 3 Rating: (0) |
I have problem in using memory SD card I am using 2GB SD card given by Siemens as compliment I am using LOG ver-7 PLC and Version 8 software. I am writing program in LADDER logic. So file name ends with ***.LLD I am able to Transfer program from PC to LOGO using ETHERNET connection cable so also from the PLC back into PC. In both cases the program is maintained in Ladder logic I mean i am getting back from PLC the program in ****. LLD. ----- Now if i try to use the MEMORY SD card to transfer program from card to PLC it says UNKNOWN CARD - Esc to get back. When i try to get back from PLC into Memory SD card it does copy program from PLC into Memory SD card. But the file name it gives is LOGO_U_P.BIN this file extension is not opening in LOGO software Help me to use MEMORY SD CARD to transfer programs into and out of PLC in LLD format
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/11/2015 1:03:20 PMNew subject after splitting |
|
5/11/2015 10:36 AM | |
Joined: 12/18/2014 Last visit: 5/5/2024 Posts: 32956 Rating: (4075) |
The file on the memory card may only ever be named "LOGO_U_P.BIN". Another file name is not allowed. |
Follow us on