2/3/2016 10:11 AM | |
Posts: 223 Rating:
|
Hello all :) I have an issue with alarm logging: I've configured some messages that have to be shown when a process value change (for example when the setpoint of a motor changes). Sometimes the message occurs when the setpoint doesn't change. See attachment for an example. The script for generating the alarms works as it should work, but apparently sometimes a bug like this one slips in :p Can anyone help me? Thanks in advance! :D Attachmentprobleem.docx (41 Downloads) |
2/3/2016 1:27 PM | |
Posts: 223 Rating:
|
schufri, What do you mean? Georg, Here is the attachment. Attachmentprobleem.docx (32 Downloads) |
Follow us on