2/23/2016 2:03 PM | |
Posts: 3093 Rating: (322)
|
Hello andreialmasan, Regards, |
This contribution was helpful to1 thankful Users |
3/3/2016 11:36 AM | |
Joined: 8/12/2009 Last visit: 10/25/2023 Posts: 27 Rating: (0) |
Hello Kaulquappe, I still have problems with the connection. I have attached 2 pics with the WinLC configuration and Station configurator. The error is 80A7 "Communications error: you have called TDISCON before TCON was complete. TDISCON must first complexly terminate the connection referenced by the ID." and then 7000."Call with REQ=0, establishment of connection not initiated" I have modified the program so that TDISCON is not called, but i had the same result. At this moment the "server" is located in the same computer(Panel PC). Database with communication parameter is also in attachment. Thanks! Attachmentpics.zip (27 Downloads) |
Follow us on