3/4/2016 2:25 PM | |
Joined: 12/28/2006 Last visit: 6/26/2023 Posts: 5 Rating:
|
Hi i need help to develop one Project..I have doubts about the use the technological motion functions. I'm using the follow devices: - CPU 1512-SP - 2 drives Simotion S120 single motor module 6SL31201TE218AA4 -1 drive Sinamics S120 6SL31201TE130AA4 - 2 servomotor 1KF70832AF711RH0-Z N05 - 1 servomotor 1FK71032AF711RA0 I need a example about to use this configuration on TIA13 and if possible use the technological functions in the CPU 1512-SP and the recommended PZD to be used in this servo. I will use positioning and synchronism functions.. I apreciate your help.Regards Mateus ------------------------------------------------------------------------------------------ |
Last edited by: Mateus at: 3/4/2016 2:27:15 PMLast edited by: Min_Moderator at: 3/7/2016 1:32:19 PMNew subject after splitting |
|
Follow us on