7/6/2009 9:52 AM | |
Posts: 8 Rating: (1) |
Thank you for that post ddg. But it is posibble to reinsert the Siemens functions to the MMC. Or I should throw it to garbage? |
7/6/2009 9:59 AM | |
Joined: 10/7/2005 Last visit: 10/14/2024 Posts: 3024 Rating: (1054) |
Hello Ionut_Robu throw it into the rubbish bin and have a look at this FAQ: Why is the MMC no longer recognized by SIMATIC devices after it has been formatted in a third-party device? |
Cheers |
|
7/6/2009 2:38 PM | |
Posts: 261 Rating: (42) |
You are welcome |
7/6/2009 3:44 PM | |
Posts: 8 Rating: (1) |
U are funny. With 2 MB of memory maybe, just maybe, I can do a photo |
3/11/2016 11:34 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by problem plc is split to a separate thread with the subject Format MMC, Error "No other active partner can be found". Best regards |
Follow us on