3/21/2016 2:10 PM | |
Joined: 7/7/2011 Last visit: 7/11/2024 Posts: 87 Rating: (4) |
I have been asked by a customer to install an archived program into a new machine when I open the project in step 7 V5.5 SP3 I get the following messages (see missing missing software packs.bmp) I have winCC2008 and Simotion scout v4.1 installed when I try to open the scout part of the project I get the message (see scout.bmp) I don't understand why it says I have version 47.52 and require 68.11 what version(s) of software do I require? are they available as upgrade downloads or do I need to purchase later versions?
Attachmentpictures.zip (43 Downloads) |
Follow us on