4/20/2016 12:59 PM | |
Joined: 12/4/2009 Last visit: 5/3/2024 Posts: 452 Rating: (134) |
Sadadhi, in that case I have a bad news for you: after deletition you will not be able to generate reports from the UA. But then again, your customer will have all the data in *.csv files, meaning that data is not lost for good. This data can also be reimported from *.csv files back to the UA, using UA editor, just like for export. But generally, I do not think that UA will slow down your WinCC startup. There is a general rule about the number of entries in the UA (320000 per archive), you might want to look at this Link to UA topic. It is possible to hold even more data, but it's not supported nor recommended. Hope this helps. Regards. |
If this post actually helped, you may consider using the Rate button above. |
|
Follow us on