1/20/2015 9:24 AM | |
Joined: 6/22/2006 Last visit: 3/7/2022 Posts: 156 Rating:
|
Hi, maybe you can use instead of IO communication TCP/IP Communication. On the SIMOTION Utilities&Applications DVD you can find the LCom library, which offers a great variety of communication services on the basis of TCP/IP for SIMOTION and SIMATIC. You can find the library also here http://support.automation.siemens.com/WW/view/en/48955385. The library LCom can be integrated into your project easily with the Project Generator SIMOTION easyProject (also included on the U&A DVD). Regards Manfred |
1/20/2015 12:33 PM | |
Joined: 10/11/2006 Last visit: 8/1/2024 Posts: 5883 Rating:
|
Hello, there is a FAQ in the simotion manual of the LCOM library. 5.1 Data transfer between SIMOTION and SIMATIC controllers 5.1.1.2 BOOL data type http://support.automation.siemens.com/WW/view/en/48955385 |
With best regards, |
|
Follow us on