3/29/2013 7:14 AM | |
Posts: 19 Rating:
|
Hello, In my Project, S7-400H with CP443-1. ( As Server) is communicating with Yokogawa DCS(As Client).Both Cable from each CP443-1 are connected point to Point to Yokogawa DCS ( 2 Ethernet Cards) . TheFirst CP443-1 in Rack-0 is communicatingwell, Error=0, Status=0, (Tx/Rx) While the second CP443-1 in Rack-1 showing Error=1, Status=16#8304, (Only Rx) I have assured that hardware is OK,cables are OK, How can I troubleshoot in this regards, Enclosed is the details of Network configurtaion, and CFC Chart Status. The Nietpro Connection status: passive connection establish. in progress. AttachmentError_description.pdf (741 Downloads) |
Last edited by: O_Moderator at: 3/31/2013 4:59 PMnew subject after splitting from /tf/WW/en/Posts/11480#top Last edited by: M Saad Khulsai at: 3/29/2013 7:17 AMLast edited by: M Saad Khulsai at: 3/29/2013 7:16 AM |
|
4/4/2013 11:24 AM | |
Posts: 3093 Rating:
|
Hello Saad, the MODB4H block is not capable of hot standby. CP443-1EX11 and -1EX20 are not capable of multiport function. Regards, Kaulquappe |
4/4/2013 12:01 PM | |
Joined: 1/9/2012 Last visit: 3/28/2024 Posts: 40 Rating:
|
Hello Saad, In your case a license 2XV9 450-1MB-11 with blocks MB_REDSV/MB_CPSRV will be required. |
6/25/2014 1:34 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating:
|
New question split intoMB_REDSV reading/writing several DB's. With best regards, Narrator1
|
11/23/2015 11:09 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating:
|
New question published by janbar_k is split to a separate thread with the subject C443-1 Adv in S7-400H. Best regards |
This contribution was helpful to
1 thankful Users |
8/1/2016 2:19 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating:
|
New question published by kakolukia is split to a separate thread with the subject Connection of two CPU 400H. Best regards |
Follow us on