(1)| 9/16/2016 2:20 PM | |
|
Joined: 6/3/2014 Last visit: 12/12/2025 Posts: 660 Rating:
|
Hello TymRyder, did you do a full compile of the HMI project (software)? Are you sure there is no other function in the PLC writing into your recipe tags? |
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
| 9/16/2016 5:35 PM | |
|
Posts: 4 Rating:
|
I have already tried a full compile, I am attempting at this moment to delete the rename/delete the IM folder and test again. But there are no other functions writing to the recipe tags. The tags are in a DB and the only other logic which addresses them is used for reading only. As you can see from the video there are variables there which set the position of a servo an boolean values which determine whether another process will or not occur but nothing is writing back to the DB from the logic, only reading. UPDATE: This did not fix the issue. Also I should note that this issue occurs just by selecting the different recipe's from the list, I do not have to press any of the buttons to download to PLC or Save or anything. Just by selecting the initial recipe from the list, then selecting another one the flickering error will occur. |
Last edited by: TimRyder at: 9/16/2016 5:45:55 PM |
|
Follow us on