10/25/2016 12:41 PM | |
Joined: 10/5/2016 Last visit: 9/12/2022 Posts: 236 Rating: (7) |
Hello ChristophD, How to add SIMATIC PC Station to the STEP7 ( Insert -> Station -> SIMATIC PC Station). Because, it is absent there as a point. How to add it there??? Even If I want to make new project I can't find it there. I know that STEP7 demands: 1) Simatic PC Station; 2) CP5512 hardware STEP7; How can help the project I can't imagine. And how to identify the necessary parts by the code ID from the screenshots above in topic? I attach customer project which I can't open and screenshots. AttachmentCustomerProject+Screens.zip (149 Downloads) |
10/25/2016 2:49 PM | |
Joined: 10/5/2016 Last visit: 9/12/2022 Posts: 236 Rating: (7) |
But I haven't found any software packages from official site SIEMENS connected with PC Station. |
10/25/2016 3:36 PM | |
Joined: 10/5/2016 Last visit: 9/12/2022 Posts: 236 Rating: (7) |
Command "s7aversx" doesn't work at cmd. OS is attached below. |
Follow us on