4/24/2008 10:32 AM | |
Joined: 9/27/2006 Last visit: 8/7/2024 Posts: 12273 Rating:
|
Hello Ton; What you are thinking of is called "Direct data Exchange", and there is a lot of information on this type of configuration on the Support webpages. Here is one particularly interesting FAQ that discusses setting up two S7-300 CPU (configured as Profibus slaves) to allow data exchanges between the two. It also comes with a sample project you can study: http://support.automation.siemens.com/WW/view/en/1016961 Hope this helps, Daniel Chartier |
4/24/2008 11:54 AM | |
Joined: 4/20/2007 Last visit: 5/27/2024 Posts: 724 Rating:
|
Thank you for the info! I'll get into it. |
4/26/2008 4:07 PM | |
Joined: 4/20/2007 Last visit: 5/27/2024 Posts: 724 Rating:
|
Thanks a lot, Ill get into that one too |
Follow us on